2013年被称为是4G元年,国内三大运营商都已经开始了4G网络的建设和测试,甚至中国移动更是开始实施TD-LTE“双百”计划,即TD-LTE网络覆盖将超过100个城市,TD-LTE终端采购将超过100万部,从而在未来建成全球的LTE4G网络。所有的一切,似乎都在向我们预示着4G时代即将来临。平安城市开启高清网络化视频监控4G时代,那么4G带来监控市场怎样的发展?
平安城市开启高清网络化视频监控4G时代
高清网络摄像机在提供给人们清晰的视觉体验的同时,也对网络带宽提出了更高的要求。以720P实时视频为例,采用标准H.264MainProfile压缩算法的高清网络摄像机至少需要2Mbps才能获得“高清”的视觉效果,而1080P全实时视频则需4Mbsp以上。普通ADSL的上行带宽早已无法满足高清视频的需要。
随着3G、Wi-Fi、专网等无线、有线宽带技术的成熟和应用,大流量数据的远程传送更加方便,这也扫除了高清网络摄像机在大范围应用中的传输障碍。目前,在平安城市、金融联网监控等项目中通常采用自建光纤网络或局域网络实现1000M带宽网络。这种千兆带宽资源,在前端安装100路1080P全实时高清网络摄像机(即使按每路占用资源4Mbps计算),占用总带宽资源不到50%;如果是采用720P传输,带宽还可以减少一半。这样,完全可以有效支持高清网络摄像机的实际应用。
在无线传输方面,3G网络加速了手机上网的速度,使可视电话、手机游戏等应用如火如荼。但在安防视频监控行业,却还没有实质性的应用。究其原因,一是3G网络建设相对滞后;二是3G资费依然太高。面对高清视频监控对于带宽的要求,3G更是力有未逮。要想真正实现高清无线视频监控,还需要等到4G的推广。目前,TD-LTE的出现,为我们开启了4G时代高清视频监控的大门。
4G监控弥补3G空白,成无线监控后备军
3G在安防市场的应用主要是利用其移动无线传输的优势,应用于移动监控领域。许多业内人士表示,一直以来,不受时间、地点、场合的约束使场景内实现视频监控一直是安防业内努力的一个方向。利用无线传输,在网络带宽允许的情况下若能实现无线移动高清传输又何尝不是一种突破呢?但是,以目前的无线监控发展情况来讲,尽管3G无线监控还存在许多弊端,但4G监控将会弥补其中的一些空白:
1、无线网络的带宽与频率资源更为有限,带宽不够不能保证监控画面质量。以3G网络为例,在高速移动的过程中传输速率为144kbps,若想保证CIF画面需求传输速率至少保证512kbps。技术不成熟,网络带宽不足是无线移动监控的致命因素。然而,4G网络可实现100Mbps的速度下载。4CIF的画质只需要2Mbps的传输速率,对比可知,也许实现无线高清监控都不在是梦。
2、由于费用过高,无线网络监控得不到广泛推广。3G视频监控资费过高,一般用户无法承受;行业用户难于承担视频监控项目后期的持续网络资费支出。但有相关人士表示,4G资费有望有较大下调,让4G网络更“亲民”。4G网络传输价格下调必将更易接受。
3、目前的3G视频移动终端还不完全适用于3G视频监控,比如在前端存储上,普通硬盘体积过大,导致整机不利于安装;4G网络建设将更灵活,全球漫游,接口开放,能跟多种网络互联,终端多样化以及能从第二代平稳过渡等特点。
3G网络建设现已基本成型,下一阶段国家将大力研发4G网络设备。2010年出台的《国务院关于加快培育和发展战略性新兴产业的决定》中提到,“到2015年,战略性新兴产业形成健康发展、协调推进的基本格局,对产业结构升级的推动作用显着增强,增加值占国内生产总值的比重力争达到8%左右”。其中就有与通信业有关的宽带网络及新一代移动通信(即TD-LTE及其后续4G标准)。2011年初,工信部通信发展司司长张峰透露,TD-LTE(国产4G技术)概念验证工作已经完成;研发技术试验阶段的测试工作正在进行,上海、杭州、南京、广州、深圳、厦门等六个城市将依次开展。海康威视(002415,股吧)产品经理林万彬也曾说过“4G已经走上日程,但是真正规模化的应用,还有待网络大范围成熟的商用。”政府的大力支持,以及企业对4G网络的期许都是前进的动力。
4G网络建设能够较好地弥补3G的不足,尽管4G也存在一定的技术短板,但是随着技术的发展我们有理由相信,在不久的将来4G网络会成为无线监控的后备军。
移动4G网络的发展趋势
尽管现在4G网络发展迅猛,甚至在国外早已经开始了大规模的商用,但同样还是存在不少缺点和不足,比如网络标准和频段上的差异,将在国际无缝漫游等方面带来诸多不便。尽管如此,从未来移动4G网络的发展趋势来看,则预计将是TDD/FDD双制式深度融合,这样使用共有的资源优点,将为用户带来更出色使用体验,例如高速移动用户优先分配到FDD网络,漫游切换和信号质量更可靠。而观看视频的用户优先则分配到TDD网络,提升频率利用率。而两种制式的互补,还可以发挥各自优势,系统动态分配资源,让用户获得好的服务。
不仅如此,网络和终端多制式深度融合也同样是4G网络的发展方向。此前中国移动已经在香港组建TDD/FDD融合4G网络,取得了丰富经验,并已经有相关支持终端问世。而随着国内建设的TDD网络规模铺开,相信也将会是支持TDD/FDD/TD/GSM多制式的网络,这必将也使得4G网络的发展道路会有越走越宽,从而为无数用户带来更好的服务和体验。