噪音来源
LED驱动的噪音来自哪里?
噪声来源来自一些磁性元件(如 变压器 ,电感器…)和多层陶瓷电容器(MLCC)。
为什么会产生噪音?
磁组件产生噪音主要有以下几个方面:
Percussion - The face of core pieces can scrape together when the magnetic flux is varied;
Collision of movable elements (bobbin, core , wire ..etc.);
Magnetostriction- The dimension of coil material is changed;
Coil self Motion-The ripple current pass through coil produces attractive and repulsive force that to move the wires.
多层陶瓷电容器也会产生噪音,原因在于:
Piezoelectric effect – Substrate vibrate with Voltage amplitude, and when the time amplitude cycle come to the bandwidth of auditory are, Harmony is recognized as a noise. Capacitor distortion transferred to the PCB acting as an amplifier。
降低噪音的方法
虽然目前我们没有方法来消除噪音,但是我们可以降低噪音水平。具体方案就是降低磁性元件的噪音水平:
Reducing peak flux of magnetic as low as possible;
Potting the PCBA;
Vacuum Varnish for magnetic parts. Method to reduce noise level for MLCCic parts;
Reduce capacitance value in a capacitor;
Add a soft material to absolved the mechanical vibration;
Replace the MLCC with a plastic film (Polypropyleneor, Polyester…etc);
Potting : Pot the PCBA.